Overview
Data is the raw material of the future. Technologies that collect, process and store data are at the heart of the data centers that proliferate around the world.
Data is processed and stored in servers found almost anywhere around the world. Applications for this new generation of hardware require advanced equipment in locations and environments not previously experienced. With the proliferation of the Internet of Things along with its industrial equivalent Industry 4.0, machines are being equipped to share information at high speeds. These machines may be in close proximity, such as in the latest smart factory, or dispersed over the great distances found in the transportation and agricultural sectors. Servers must deliver the speed and data rates needed to ensure the greatest reliability and lowest latency regardless of location around the world.
This creates the need for highly flexible solutions. Engineers are keen to benefit from the improved performance of the latest data networks, and they need to be confident that their equipment can keep pace with their demands. The latest server and storage solutions will need to offer flexibility and scalability to support higher performance at the speed of innovation.
Molex helps solve the most complex data center challenges by collaborating early in the design process, delivering unparalleled engineering expertise, and providing industry-leading high speed interconnect solutions.
By the Numbers
75 Billion
Connected Devices by 2025
27 Zettabytes
Global Data by 2025
112 Gbps
Current Data Rate